Part Number: LM25118-Q1
Other Parts Discussed in Thread: LM25118,
Tool/software: WEBENCH® Design Tools
Dear TI Support,
I'm using the LM25118, I designed a custom design using WEBENCH Power Designer TOOL and extract the schematic file to Orcad.
In order to check the Gain Margin and Phase Margin in both Mode (buck mode and buck boost Mode).
My input voltage rage is : 6V - 18V
Output Voltage : 12V
Output current : 2.4 A
Firstly I need to know what's the input Voltage that i should using for each Mode?
secondly i have simulate the design with an AC inpute =14V, but I can't get the phase margin and the Gain margin?
Could you please check in the attachement my design and please let me Know what's the problem?
With Thanks and Regards,
Rana