Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
Hi team,
I'm planning to verify using the IBIS model of SN65LVDS100.
I downloaded the IBIS model, there are two things I want to check.
#1
Y, Zpin output signal is constant regardless of Receiver Input signal of A, Bpin.
I investigate the cause, but is there any possibility that this model is fixed output?
We will use it about 100MHz.
#2
The variation of the model is NA, but is there model specified for MIN / MAX?
Since we want to confirm that there is no problem even in the worst condition, we want to obtain a model with min / max.
Best regards,
Tomoaki Yoshida