Part Number: LM25145
Tool/software: WEBENCH® Design Tools
Hi team,
My customer is simulating the LM25145 on Webench with a 49.9k Ruv1 and a 7.15k Ruv2 for a UVLO around 9.5V. However, when they run an input transient simulation it seems to regulate the output with Vin as low as 6V (see below). Does the model used for the input transient sim take UVLO into account?
Thanks,
Antonio