Part Number: TIDA-00951
Sir,
In Page.3 of the reference design document of TIDA-00951, under key system specifications, in the back-up mode, the bus-current is mentioned as 5A. Whereas in the battery charger mode, it is mentioned input bus current is 60A. The load connected to DC Bus during testing is also drawing 5A only. Please clarify the 60A Bus input current mentioned in the table. Is it supposed to be a typo error?
Thanks and Regards,
Swathika Rao