This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
My customer will design 12W power surpply with high efficiency and small footprint.
they think using UCC28704 or UCC28700 and UCC24636.
I found PMP15002 using UCC28704.
Are there the reference design using UCC28700 and UCC24636?
Yokota-san,
Thanks for your interest here.
If you have not seen already please also look at these designs:
I'm not sure of your application but UCC28704 can support high efficiency even without Synchronous Rectification so a diode rectifier with UCC28704 might also be an option for you.
I found 1 design with UCC28700 and UCC24610 and have attached the BOM and schematic here. I don't think this design was tested though so can't guarantee performance: