Part Number: TIDA-00287
Other Parts Discussed in Thread: TUSB4041I, TUSB8020B, TUSB8041A
Hello,
I use the UP-Core. Fore some reasons I build a new Circuit for these Chip.
The new circuit should have two more USB 3.0 ports.
Is it pissoble to use these reference Design http://www.ti.com/lit/ug/tidu428/tidu428.pdf ?
with these design I would like to bring the two USB3.0 ports too the PCIE of my 100 Pin-Exheat at the UP Core.
Could someone help me?
friendly regards
Mario