Part Number: TPS61236P
Tool/software: WEBENCH® Design Tools
Hello,
I want to test the IC TPS61236P for my project requirement , while i simulate the reference design it shows schematic in simulation window without load connected also current source connected to it.. while actual schematic is with load as shown in attachment image 1..
so the problem is during simulation i get IRload equals to current source value but if i copy the same design and simulate it then the graph shows 0.25Amps curent at the load..
why the reference design is showing that current source in place of Load???