This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA/Spice/LMV761: Input Bias Current Above Common Mode Input Range

Part Number: LMV761
Other Parts Discussed in Thread: TINA-TI,

Tool/software: TINA-TI or Spice Models

I am using an LMV761 Spice model provided by TI and I am seeing something in the simulation I don't understand. My application uses a 5V supply for the device and I have a situation where the (+) input is within the -03 to 3.8V common mode input range, while the (-) input goes to 5V at the input of a 1K series resitor.  The simulation shows the LMV761 input bias current increases greatly when the 3.8V common mode input voltage is exceeded, and I am seeing a 1.15V drop across the 1K series resistor, or 1.15 mA bias current with 5V applied to it. This is in direct conflict with Figure 4. "Input Bias vs Common Mode at 25°C" of the data sheet. 

Is there something wrong with the Spice model. I'm assuming the actual device bias currents meet the 50pA limit as long as the supply voltage is not exceeded. Is this correct.

Thanks,

Doran Akutagawa