This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Gate Drivers for Solar Inverter Application



Hi.

I hope someone can answer my queries regarding my 3.5kW grid -tied dual stage solar inverter design. Currently, I am using IGBTs and ISO5000 for isolated gate driver supplies. I want to know what is the best gate drive supply.

Firstly, GaN FET are starting to replace silicon based IGBTs and MOSFETS. Also, you have suggested a possibility of using GaN FET in solar inverter application in the blog "Rethink your solar inverter with GaN". So, should I replace IGBTs with GaN FETs. If so, what would be the gate drive solution for GaN FETs.

If I continue using IGBTs (switching frequency is 15-20kHz), is ISO5500 good or would you recommend some other gate drive solution. 

There are plenty of options available on TI's website - for single channel,, dual channel and full-bridge gate drive supplies. Which one would be ideal to use. Can you please suggest with relevant reasons?

I would be grateful for your response and suggestions.

  • Hi Rushi,

    Thank you for your question. I have assigned the appropriate engineer to answer to your question.

    A few questions : Are you still planning on operating the FETs between 15-20kHz if you use GaN?
    GaN is used at higher switching frequencies while maintaining desired efficiencies for a wide range of input and output voltages.

    Have you taken a look at SiC FETs? Here is a TI-design, TIDA-01606 for a solar string inverter using SiC.

    regards,
    Mateo

  • Hi Mateo,

    Thanks for your reply.

    Surely GaN would be used at 3 to 4 times the switching frequency compared to a normal IGBT.

    Also, thanks for giving the reference to the SiC FETs. I had a look at it and I now I am more confused what to use.

    I have structured all my doubts in the point form so that it becomes easy for you and your engineer to answer.

    1. From my understanding based on what I have read - GaN FETs are better than SiC in terms of efficiency and possibility of higher switching speeds. Am I right or am I missing something?

    2. My Solar Inverter is targeted for the Indian market where I would be competing with multiple companies who import solar inverters from China. They are less costly and that is the main reason it sells in the market. So, if I would be switching to GaN or SiC, will the cost increase or decrease. Though GaN and SiC are costly, I would be saving money on size of heat sink, packaging cost and magnetics cost. But, I am not sure how would the overall cost be affected. Maybe your experience will help me in getting some idea.

    3. What technical difficulties I may face in switching to GaN or SiC based FETs. I believe one of them would be achieving the EMI standards as we are shifting to higher frequencies. Any other issue that I may face?

    4. The integrated GaN power module available on TI is rated 600V 12A. For a 3.5kW solar inverter, I would have to use them in parallel to achieve the desired current (240V rms is the grid voltage and for power level of 3.5kW, I would need a peak current of 20.6A). OR are there any other GaN FETs available for the power levels that I want to achieve OR some other solution that you may suggest.

    5. Lets say I stick to the silicon IGBTs with switching frequencies upto 20KHz. What would be the best gate drive solution? Is ISO5500 good enough or do you have a better suggestion for me.

    6. I believe GaN and SiC have not been widely adopted. Am I right? If so, what is the reason? Or what do you think is the potential of GaN and SiC FETs.

    7. Lastly, what according to you would be the best solution for a solar grid-tied inverter for a power level of 3.5 to 4 kW? (taking into account cost, ease of implementation, future scope of technology, etc)

    I have tried my best to put forward my doubts clearly. I will wait for your answers.

    Regards,
    Rushi
  • I look forward to an answer for my queries. It will help me in designing a good inverter.
  • Hi Rushi, 

    Please see the attached white papers on GaN to help you with your designs: 

    http://www.ti.com/lit/wp/sszy017/sszy017.pdf

    http://www.ti.com/lit/wp/slyy070/slyy070.pdf

    regards,
    Mateo

  • Hi Mateo,

    I have already gone through these white papers. They do mention that GaN is at a pretty nascent stage for power applications.

    Yet, they do not answer the questions that I have asked above. I am still confused and my queries above remain the same.

    I hope you can answer them.

    Looking forward to specific answers to my questions.

    Thanks,
    Rushi
  • Dear Rushi,

    TI GaN solutions such LMG3410 are fully integrated devices with built-in gate driver and protection. No external drivers are required.

    Thanks,

    Masoud

  • Hi Masoud,

    I have gone through the datasheet of LMG3410 and I understand that no external drivers are required. Is ISO7831x necessary for isolation if I am using a flyback converter to supply the isolated 12V supplies?
  • Hi Rushi,

    This will depend on your power converter topology and system grounding scheme.

    Thanks.