Other Parts Discussed in Thread: UCC27531, TPS61170
Hi SIR,.
Is it possible for cost down UCC27531 instead of BJT, TPS61170 for charge pump?
or one of the parts for this reference besides ultrasonics,..
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi SIR,.
Is it possible for cost down UCC27531 instead of BJT, TPS61170 for charge pump?
or one of the parts for this reference besides ultrasonics,..
Hello,
TPS61170 generates 30V
UCC27531 is a high side driver. 30V is supplied to the UCC27531 via TPS61170.
UCC27531: "its main purpose is to create a 50% duty cycle 30V square wave pulses to excite the transducer. There is one main reason why we used a driver IC instead of a simple circuit consisting of transistors to step up the transmit pulses. The driver ICs offer integrated shoot-through protection, which is needed because shoot-through has two consequences:
a. It drains the output caps of the boost converter quickly. We would need a boost converter with much more power to compensate for these losses.
b. It could simply thermally destroy the transistor stage. "
Is this what you are looking for ?, if not, could you elaborate your question.
further details on Fluid level sensing can be found under