Part Number: TIDA-01495
Other Parts Discussed in Thread: UCC24612
I was wondering how the UCC24612 in the Synchronous Rectifier Driver section in the TIDA-01495 reference design gets it's power. It looks like VDD for both chips are connected to each other but nothing is supplying it. I also checked the sample board layout just in case I missed it on the schematic, but nothing is connected except the two VDD pins and the bypass capacitors. I checked the datasheet and it specifies VDD be connected to 4.5V-28V.
Any help would be appreciated.
Regards,
Sebastian