Other Parts Discussed in Thread: TPS40055
Hi TI,
in the TPS40055 there must be several errors:
Look at the BOOST-Pin, that is connected over an resistor direkt to the SW-node. (In the Desktop Version it is correct connected over an capacitor)
Look at the SW-Pin that is connected over an capacitor. (In the Desktop Version it is correct)
The Feedback network has different resistor and capacitor names as in the desktop version. Additionally I think that they are displayed in the
wrong place. I know that because I tested the desktop version, in which I get a good phase margin. When I try that in the online version I get a negative phase margin. Ok I am not sure what is wrong there because it is very crazy.
Last: Are you sure the resistor on the ILIM-Pin is calculated correctly? For 2.82A I calculate myself 7.75kOhms. But the SwitcherPro gets 1.78kOhms. What is right?
Thanks a lot. (The Desktop Version works in a way I like)
Greets
Bernd