This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA/Spice/LM5085: EMI of TI's DC/DC

Part Number: LM5085
Other Parts Discussed in Thread: TINA-TI,

Tool/software: TINA-TI or Spice Models

Hi,

I am a new user of TINA TI Spice simulator.

I usually use LTPSICE but i would like to use TI spice model into TINA in order to simulate EMI of the LM5085 DcDc PFET buck converter.

I created the full schematic and I place the LM5085 transient model :(bottom of this dialogue window)

When I want to check the output transient voltage (VM1) I have 0V DC instead of square waveform with overshoot.

So, I wonder if this is could be caused by the importation of TINA spice model of LM5085.

Do you have a generic protocol in order to create a new TI component and associate its TINA spice file ?

Thanks a lot for your answers,

Sincerely,

Olivier D.

LM5085_switching_emissions.TSC