Hi!
We have developed the PCB and while testing we encountered the following error in the board :
The IC U12 - TLV1117-33IDRJR should give 3.3V output from input of 5V. But it doesnt seem to give the expected output. When we compared the schematics of 00951 and 01280, there seems to be a schottkey diode connected between the output and input in 01280 design. Can you pls clarify if the schottkey diode should be added or not to get 3.3 V output from the IC??
Swathika Rao