Other Parts Discussed in Thread: TINA-TI, , SN74AUP1G06
Tool/software: TINA-TI or Spice Models
The design under analysis uses SNJ54LS06FK part, searched for this number in the TI list of TINA models and the closest part found is SN74ls06.
I down loaded the SN74LS06 model and the extension is .isb, changed this to .cir, opened TINA-9 selected File - Import - PSpice Netlist (*.cir)... and selected the downloaded file SN74LS06_IBIS Model_SDLM014A
folder which contained the sn74ls06.ibs (changed to .cir) model and the netlist editor rejected the file.
Questions are:
Is the SN74LS06 model close to representing the SNJ54LS06FK part for use in a critical aerospace application?
Is there an existing model that would be accepted into the TINA-9 library of IC parts?
If the SN74LS06 model the only one existing, how do I get this model into the TINA-9 library for schematic generation?
Thanks for any assistance you can offer.
Regards,
James Williams