Part Number: LM5122
Other Parts Discussed in Thread: TINA-TI
Tool/software: TINA-TI or Spice Models
I am having the same irregular circuit error that many others seem to have. I'm not sure why my circuit is giving me an irregular circuit error when I try to run a transient analysis. It specifically states "Component/Terminals: .T1 6". This doesn't make any sense to me, because net 6 isn't connected to T1, and neither T1 nor net 6, which is the IC's syncout pin, seem mal-formed when I export and view the netlist. Am I misunderstanding the error message?
Thanks,
PaulLM5122 Sepic.TSC