This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00779: tida-00779

Part Number: TIDA-00779

How Rsense resistor is calculated in TIDA-00779 3.5KW PFC? As per calculations from reference deign note , Rsense should be 0.008Ohm but in the Schematic Rsense resistors (R4, R5, R45) are shown as 0.0033ohm( 0.01Ohm/3; As 3 resistors are parallel)