Part Number: TIDA-00489
I am using the TIDA-00489 reference circuit as the basis for my design using the same BOM. The Murata PIR detector part does have a lens installed. Unlike another user who did not see any activity without the lens installed, I do see activity regardless of the lens installation. "Activity" means that I see transitions on the PIR_OUT_HI and PIR_OUT_LO. When I walk back, I see the last stage of analog (
R19) is moving between the voltage extremes. The comparator stage looks like it is working fine and outputting a valid signal for what's fed to it.
I have used a "fresh" PIR sensor that has always been covered with a lens - so it has no scratches or fingerprints - with similar results. Power integrity is key - this design runs off of 2 AA batteries (3V) which also powers other circuitry. I have ensured that the other circuitry is OFF to avoid any crosstalk issues or power dips (power integrity) due to "high" current demands of other external circuitry.
The purpose of the PIR is to "wake up" the rest of the circuitry - so none of that other circuitry is active when the PIR is operational. The problem is the PIR is constantly "firing off" - so I synthetically keep the rest of the circuitry from waking up when PIR_OUT_[HI,LO] transition (ignore transitions).
I see some periodic (not at any given regular period) high frequency noise on the PIR Vin side. I am going to attempt to correlate this with the PIR's amplified output (low frequency swings back and forth) to see if these short bursts of noise correlate with the movement on PIR or not. In order to see these, I set the vertical (Voltage) offset to center on Vin of the PIR and then turn the scale way up to make the noise more evident.
I am wondering if there were ever issues with the "high impedance" Vin to the PIR. A series 619k as part of an RC filter is different from Murata's reference (
) which uses a 1ohm series off their regulator (w/22uF cap). Experimentally, I could shotgun a lower R value for the power series ("pull up" of the RC filter) - but I was wondering if this has been seen as a general problematic area. My assumption is that the circuit is low current enough that the R value scales according to the current consumption of the TI parts vs. the Murata design (NJR parts).