Part Number: PMP9594
Hi ,
we would like to try PMP9594 design based on UCC28722 for 5V .1.5 Amp Power supply .
refer PMP9594 . we do need Transformer core and winding details for G144011LF ( GCI make ) detail to start with . pls help to share .
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PMP9594
Hi ,
we would like to try PMP9594 design based on UCC28722 for 5V .1.5 Amp Power supply .
refer PMP9594 . we do need Transformer core and winding details for G144011LF ( GCI make ) detail to start with . pls help to share .
Hi Nandakumar,
I do not have the core and winding information for the transformer, but here are the electrical specs:
-
- Switching frequency ~75kHz
- 14:1:3 ratio (primary:secondary:bias)
- 900uH primary inductance
- Primary current ~ 500mA (peak) and 150mA (rms)
- Secondary current ~ 2.6A (rms)
- Shield winding
regards,
Brian