Part Number: TIDA-00484
Other Parts Discussed in Thread: HDC1010, CC1310, ENERGYTRACE
Hello!
How long TIDA-00484 was tested under -20 degree C?
I tried to produce the same device (without boost DC-DC, Timer and Switch, using CC1310 Standby-Mode only). I set transmit period to 1 second (1 send every second) and put device in freezer under -20 C. Estimated life period was 40 days (confirmed by EnergyTrace and Fluke 87V), but device died after 5 hours (used Energizer CR2032). I tried to increase bulk capacitor capacity to 230 uF - no success. Tried to limit battery discharge current to 3 mA (using resistor after battery), disconnect HDC1010, upload simple code from example EasyLinkTx to make sure, that it's no problems in code - no success.
In room temperature - all ok.