This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01093: Use a BQ76940 and a BQ76930 to support up to 24-Series cell application

Part Number: TIDA-01093
Other Parts Discussed in Thread: BQ76930, BQ76940

Dear TI experts,

TI has a reference design of 2 BQ76930 to support maximum 20-series cell application, and I intend to design a system to monitor up to 24-series cell application. Also,I want to minimize the cost.

I wonder if I can use one BQ76930 and one BQ76940 for 24S cell application just like TIDA-01093 Reference Design.  

If so, what should I pay attention to?Or just like TIDA-01093 Reference Design?

I wish your early reply.

Thanks & Best Regards