Tool/software: TINA-TI or Spice Models
Is it possible to get an automated y axis in tina-ti? In ltspice the y axis is selected automatically in the transient selection. The x axis is ok because it is the time axis and you select this yourself.
In tina you have to adjust the y axis. for instance I am getting a y axis up to 300v when the simulation result is 24 volt so I have to select an axis of 0 to 30v. even then I can only tell that the line is 24v by looking across to the y axis. shouldn't there be a probe to place on the ouput line to give the exact voltage?
Hoping you can assist to make my simulations easier in tina -ti. I actually find ltspice much easier to use but in the particular circuit I have built this does not have the components I am using.