Part Number: TIDA-00653
Other Parts Discussed in Thread: UCD3138
I'm currently experiencing some issue when programming/flashing the device. The adapter used is USB Interface Adapter EVM, with Fusion Digital Power Studio.
The adapter is recognized by PC (green LED and SSA detached/re-attached message), as well as outputting appropriate signals through the ribbon cable (verified using logic analyzer). However, the board (fabricated using the Altium output files provided) doesnt respond.
The message I'm getting is 'No device found', or 'No ROM detected, device maybe in flash mode'. Scan using Device ID, Device Code and PMBus Revision return NACK, along with 'USB/SAA Error'
All the connections are secured, and I did try various bus setting (100 kHz and 400 kHz, and pull up settings on the communication lines)
The UCD3138 receives sufficient power, and outputs 1.8V at BP18 (pin 58), the DPWM pins are low on power up, so I assume it's working correctly, also we have multiple boards that are having the same issue.
I installed the driver provided for this board, and research similar problem on the forum, but none solved the problem for me so far, the UCD3138s are fresh
Do you have any suggestions regarding this problem?
Thanks,