Part Number: TIDA-01168
Other Parts Discussed in Thread: LM5170-Q1
Hello,
When lower power for example 200W and we want to optimize the design, what we can do?
Single-phase configuration is enough? I think TIDA-01168 max current for each side are 41.5Arms for 12V side and 10.5Arms for 48V side.
We expecting 12V side (acutal usage is lower voltage) is 60Arms and 48V side is 4.2Arms.
It seems to be able to make the system by single-phase. Is my understand correct?
Best regards,
Toshihiro Watanbae