Hello,
Checking TIDA-01371 design, I have some questions:
1) There are two VCTRL inputs to set the positive and negative regulators. Why is it two inputs? Why not making a tracking negative regulator, or why not both set by single VCTRL.
2) The feedback loop for positive output sets the "positive virtual ground" and the positive output is this voltage plus positive regulator output which is +3.3V. But the feedback loop for negative output sets the negative output. Why are these loops different.
3) the regulators are set to +3.3V DC, what are the selection criteria for this voltage?
4) The regulators are selected to be very low noise, obviously the output noise is the sum of noises of regulator section and virtual ground section. What is the noise value and stability of virtual ground section?
With Regards,
MHG