Hi,
I would be very grateful if you could help regarding a SwitcherPro question.
Switcher Pro is set to simulate a TPS61170 with the following settings:
Voltage input minimum 15 volts
Voltage input maximum 15 volts
Output voltage 38 volts
Output current 0.25 amps
The simulator shows an output capacitor C4 of 4.7 uF. An output current of 0.25 amps gives a load resistance
of 152 ohms.
The loop response indicates a dominant power stage pole at 222 Hz. However if I use the formula from
page 16 of the TPS61170 datasheet for a current controlled boost converter I get 445 Hz which is twice the value.
Many thanks for your help.
Nigel