Part Number: PMP11287
Other Parts Discussed in Thread: UCC3813-0, PMP20708
Hi, Everyone
My customer is requesting the following power supply.
Input:
AC: 10.2 to 126.5V 50/60Hz±5%
DC: 10.2 to 126.5V
Output
DC 12V (about 70mA) or DC 5V (about 170mA)
AC: 10.2 to 126.5V 50/60Hz±5%
DC: 10.2 to 126.5V
I would like to modify PMP11287 circuit with reference to it, but how should I modify it ?
Best Regards,
Masami