This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TLV62569: WEBENCH - TLV62569 Simulation (3.3V Output)

Part Number: TLV62569

Tool/software: WEBENCH® Design Tools

Hello,

I tried simulating TLV62569 on the WEBENCH by using the part search function - The WEBENCH autofills the input and output parameters (input: 2.5-5.5V and output: 1.8V, 2A) -- But I want to change the output to 3.3V. I change the output to 3.3V and click "View Design" and it still simulates at 1.8V at 2A, see screenshot.

I tried changing the Output from the "Customize" and "Update Design" page and it says "Design Updated", but does not update the schematic or the "Output: 1.8V at 2A" header. See attached screenshot.

How can I get the output and schematic to change to 3.3V output at 5V nominal input?