Part Number: TIDA-01480
Other Parts Discussed in Thread: TPS65023, LM3881
Hi!
Regarding the TIDA-01480 design.
I wonder how the power-supply sequencing to the voltage supplies work. It is not documented in TIDUDN1B.
Im looking at the assembly variant 001 for Xilinx ZU2CG device.
In the schematics there are passive components to delay the on/off times for different enable signals on page 6.
I cannot figure out how the TPS65023 (U1) is enabled at start-up. VLDO2A_3V3 output is connected to VIO via an "0"-ohm resistor.
VIO feeds the nets on page 6 for different enable signals.
How is the output VLDO2A_3V3 enabled at power-on. Do I need an external enable to start-up?
Br Mikael