Part Number: TIDA-00284
Other Parts Discussed in Thread: TIDA-00289, , TIDA-01250
Hello,
Application in our company's machines require a section of solenoids which are pushing an object against the transportation band during certain process (up to 80-90 solenoids at one time each with same stroke, approx. 10mm) . The application requires the ability to regulate solenoid's hold force in possibly wide range (pull & hold application) and it should be possible for each solenoid independently as well as for whole sections. Controling unit needs to be ready to associate (connect) to industrial PLC which will set actual required force for each solenoid, feedback for PLC regarding present state of each solenoid is required, communication with PLC is preferred to be via one of communication protocols e.g. Modbus. We are interested in long-term cooperation in term of mentioned drivers.
Please contact me with info regarding your ability to supply this application,
Best regards
Wojciech Szczepański