This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi.
We are trying to combine TIDA-01187 with 01573 for high-speed & narrow pulse width LIDAR.
The whole frame structure is surely TIDA-01187, but some parts in each design are not compatible when they are totally integrated.
For example, as I know, GaN LMG1020 driver already has a role similar to DAC5682Z in the TIDA-01187.
Is it possible to combine the TIDA-01187 with 01573? If possible, how can I do it? Thanks!
Hi Minseong,
The TIDA-01187 and TIDA-01573 were done by two different groups. The two TIDA's are not designed to be compatible with each other. But I think you should be able to replace with TX on TIDA-01187(TSW1400 + DAC5682Z + OPA695) with a pulse gen and TIDA-01573.
Regards,
Neeraj
Thanks! Also, can I get TSW3080 Schematics or product? The schematic is not included on the supporting design files ;)
Regards,
Minseong