Other Parts Discussed in Thread: CC1310
Hello!
I'm trying to implement TIDA-01212 in my design and have some questions:
1. According to Vishay site,TSPF6200 IR LED is not available. Can you advise a similar LED? I can't find "Relative Spectral Sensitivity" parameter on other IR LEDs. I also tested 15 different LEDs (850-950 nm), TX part works fine, but not RX (i can see pulses on DIO28 (using oscilloscope), but voltage did not drop less then 2V).
2. That is the purpose of R2 resistor? GPIO max current is 8 mA, that is much less then LED limit.