Other Parts Discussed in Thread: OPA695
Hi
I try to simulate a circuit using a downloaded model from the TI website.
When I added the model to the schematic symbol and mapped the ports.
When I run a simulation I get an error message:
[Error] TXfilter XSpice Error: Syntax error in expression on line: 93
The error found is in the line:
E_ABM21 $N_0001 0 VALUE { ( V(Dis) / (V(V+) + 1e-6) ) * 5.0 }
I have no clue what is wrong but I attached the model part of my simulation.
Hopefully one of the other users could help me get this simulation running. I do not need the disable pin in my simulation I am currently only performing an AC tranfer sweep.
Thans in advance.
Bert Hennink
*Models and Subcircuits:
.SUBCKT OPA695_model + - Dis OUT V+ V-
.PARAM x1 = {1/8}
.PARAM x2 = {x1*2}
.PARAM x3 = {x1*3}
.PARAM x5 = {x1*5}
.PARAM x12 = {x1*12}
.PARAM x16 = {x1*16}
.PARAM x60 = {x1*60}
C_C1 Vmid Dis 2p
X_S1 $N_0001 0 $N_0002 $N_0003 OPA695_model_S1
R_R11 Vmid Dis 100MEG
R_R8 Vmid $N_0004 10k
Q_Q1 $N_0006 $N_0005 $N_0007 PNP8 {x1}
Q_Q4 $N_0008 $N_0008 $N_0005 NPN8 {x1}
Q_Q5 $N_0009 $N_0005 $N_0010 PNP8 {x2}
Q_Q12 $N_0011 $N_0005 $N_0012 PNP8 {x2}
Q_Q9 $N_0013 $N_0005 $N_0014 PNP8 {x2}
Q_Q7 $N_0015 $N_0015 $N_0016 NPN8 {x2}
Q_Q6 $N_0015 $N_0017 $N_0009 PNP8 {x16}
Q_Q14 $N_0011 $N_0017 $N_0018 NPN8 {x1}
Q_Q16 $N_0017 $N_0018 $N_0019 NPN8 {x1}
Q_Q15 $N_0018 $N_0018 $N_0020 NPN8 {x1}
Q_Q10 $N_0011 $N_0011 $N_0021 NPN8 {x16}
Q_Q8 $N_0013 $N_0015 $N_0022 NPN8 {x2}
D_D3 $N_0023 $N_0021 DX 1
D_D1 $N_0021 $N_0024 DX 1
D_D2 $N_0024 $N_0025 DX 1
Q_Q18 $N_0026 $N_0026 $N_0021 PNP8 {x16}
Q_Q17 $N_0026 $N_0015 $N_0027 NPN8 {x2}
R_R24 V- $N_0028 250
X_F1 $N_0002 $N_0029 $N_0006 V- OPA695_model_F1
Q_Q2 V- $N_0006 $N_0005 PNP8 {x1}
R_R18 V- $N_0015 50k
R_R20 V- $N_0022 500
R_R19 V- $N_0016 500
R_R21 V- $N_0019 2k
R_R22 V- $N_0020 2k
R_R23 V- $N_0027 500
D_D5 $N_0028 V- DX 1
Q_Q20 $N_0030 $N_0030 $N_0028 NPN8 {x3}
Q_Q19 $N_0030 $N_0026 $N_0025 PNP8 {x16}
Q_Q25 $N_0031 $N_0030 $N_0032 NPN8 {x12}
Q_Q24 $N_0034 $N_0033 $N_0035 PNP8 {x12}
R_R10 V+ V- 123.609k
E_E1 $N_0004 V- V+ V- 0.5
E_ABM21 $N_0001 0 VALUE { ( V(Dis) / (V(V+) + 1e-6) ) * 5.0 }
R_R9 Dis V+ 41k
R_R12 $N_0008 V+ 8k
R_R14 $N_0010 V+ 500
R_R15 $N_0014 V+ 500
R_R16 $N_0012 V+ 500
R_R17 $N_0006 V+ 72k
R_R13 $N_0007 V+ 1987
Q_Q21 $N_0036 $N_0030 $N_0037 NPN8 {x5}
R_R7 $N_0029 Vmid 10k
R_R25 V- $N_0037 150
D_D7 V+ $N_0038 DX 1
R_R26 $N_0038 V+ 250
Q_Q22 $N_0033 $N_0033 $N_0038 PNP8 {x3}
R_R27 $N_0039 V+ 150
Q_Q23 $N_0036 $N_0033 $N_0039 PNP8 {x5}
D_D8 $N_0039 V+ DX 1
Q_Q13 $N_0017 $N_0006 $N_0013 PNP8 {x1}
Q_Q30 $N_0041 $N_0040 $N_0036 NPN8 {x1}
Q_Q31 $N_0042 $N_0040 $N_0036 PNP8 {x1}
V_V1 $N_0003 Vmid 2.04V
L_L1 + $N_0021 1.3nH
Q_Q11 $N_0033 $N_0011 $N_0025 NPN8 {x16}
D_D4 $N_0025 $N_0023 DX 1
L_L3 $N_0040 OUT 1.3nH
L_L2 $N_0025 $N_0043 1.3nH
C_C2 $N_0036 V+ 0.2p
R_R31 $N_0043 - 65
Q_Q32 $N_0044 $N_0044 $N_0041 PNP8 {x60}
Q_Q33 $N_0040 $N_0044 $N_0041 PNP8 {x60}
Q_Q28 $N_0045 $N_0045 $N_0042 NPN8 {x60}
Q_Q29 $N_0040 $N_0045 $N_0042 NPN8 {x60}
Q_Q35 $N_0045 $N_0031 $N_0040 PNP8 {x60}
Q_Q34 $N_0044 $N_0034 $N_0040 NPN8 {x60}
Q_Q27 $N_0042 $N_0036 $N_0034 PNP8 {x60}
Q_Q26 $N_0041 $N_0036 $N_0031 NPN8 {x60}
R_R28 $N_0035 V+ 62.5
D_D6 $N_0037 V- DX 1
R_R29 V- $N_0032 62.5
V_V3 V- $N_0042 0.2V
V_V2 $N_0041 V+ 0.2V