Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
The TPS65400 TINA model on the web says it is a "Transient" Model in the link and in the Macro notes. But in the notes for the TINA transient simulation (slvm03.tsm - also on the web) it says it is an "Average" model used to do Transient simulations. Then it goes on to say it doesn't show switching ...
In the past I have understood a "transient" model to include switching and be used for startup and load step/dump type sims while the "average" model is used for AC/BODE type analysis.
1) What is this model really - transient or average?
2) Customer wants to do both an AC/Bode analysis for stability and a load step response. Can we do these with this one model?
3) There is both a Transient and an Average model available for Pspice on the web. Per the conflicting information above which is which and what is it used for?
4) Can these PSpice models be made available in unencrypted form or can the missing model be made available in a TINA.tsm form? We would like to import both into TINA.
Thank you for as rapid a response as you can give this.