This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA/Spice/UCC28700-Q1: Multiple Isolated Output, Auxiliary Supply Reference Design for DC-DC Power Supply

Part Number: UCC28700-Q1
Other Parts Discussed in Thread: TINA-TI

Tool/software: TINA-TI or Spice Models

I am using UCC28700QDBVR-Q1 for designing four isolated output of 12 Vdc & 0.2 A each.Below are design goal parameters

Vin (min)= 250 Vdc

Vin (max)= 400 Vdc

Vout1, Vout2, Vout3, Vout4= 12 Vdc each

Iout1, Iout2, Iout3, Iout4= 0.2 A each (i.e total 0.8A)


Is there any sample TINA simulation file or schematic available for the same.