This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA/Spice: Tina90-TIen.9.3.150.328

Other Parts Discussed in Thread: TINA-TI

Tool/software: TINA-TI or Spice Models

This is the same question as someone ask 3 years ago. And I has an exactly same question. I don't know how to resolve this kind of problem even though I already read the answer for the past question.

Here is my question.

I'm trying to use Tina-TI for the 1st time. I downloaded and installed the program successfully (Win10 & Tina90-TIen.9.3.150.328).

After creating a simple circuit schematic, I tried to do a transient analysis and consistently got the following error:

Error: Cannot create file "". The file name, directory name, or volume label syntax is incorrect.


How can I resolve this kind of problem?

The past answer for this kind of problem is like below.

"For some reason, the security settings for the Tina-TI Temporary Folder (Environmental Variables) were not set correctly. Once permissions were "Allowed", then
Tina-TI started working correctly."

Then how can I make 'permission' be allowed?

Please tell me the solution for this.

Thanks

  • Hi JEONG,

    Please do the the following steps which may resolve the issue you are facing:

    1. Go to the options highlighted in red coloured box in the snapshots shown below and clik on them following the sequence as :(a) View (b) Environment variables (c)Temporary Folder

    2. Once you click on  Temporary Folder it will open a window with default TINA version installed in your machine,Right click on it to get properties and click on it.

    3.Once you click on properties you will get following window,click on Security marked in red coloured  box.

    4.Once you click on Security you will get following window,click on Edit marked in red coloured  box.

    5.Once you click on Edit you will get following window,Untick  Deny and tick Allow marked in red coloured  boxes ,then  Apply it and  run the simulation.

    Please let me know if you are still facing the issue.

    Best Regards,

    Ashis