This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00779: 3.5-kW PFC Inductor parameters

Part Number: TIDA-00779


Hello!

Can you help me out with pfc inductor parameters (L1)? It seems to be a typo somewhere: in the tidube1c 2.33 (6) it is calculated to be 180uH. In the BOM it's 790uH. And on the photo of the assembled board it seems like it's even more. Based on the approximate number of turns on the photo it seems closer to the 790uH, but I can't find a core with low permeability to achieve that.