This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Battery protection circuit for a solar battery

Other Parts Discussed in Thread: LM5060

I want to build a battery protection circuit for an e-bike which will limit the current to 125A but will not cutoff if the current is exceeded.The battery voltage is 48V and is charged using solar energy. Which Current limiter or IC can I use?