This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TIDA-01580: TIDA-01580

Part Number: TIDA-01580

Tool/software: Code Composer Studio

Hello Sir, Mam,

My question is about replacing the ARM MCU with TI RF430152H. Is it possible in that case what I should be aware.

Our development and environment is based in NFC rather than BLE and I need to get to work in this direction.

On current I`m working on an algorithm for a medical class Blood pressure using the MCU RF430152H and PPG. 

I see that the board TIDA-011580 will be a good test bed to get test results, but our goal is to get the patient monitor arround the above mentioned TI MCU.

I`m very Grateful for the help you could provide me.

Sincerelly yours,

Nestor Ramallo

 

  • Hello Nestor,

    Thank you for reaching out.

    We haven't done any comparative study between the two devices for this application. But I would recommend comparing the memory sizes and GPIOs. Are you planning to use the same AFE for the PPG measurement?

    I can help you with the schematic review for AFE section, if required.

    If you need the code for TIDA-01580, please check the design folder on http://www.ti.com/tool/TIDA-01580

    Regards,

    Sanjay R. Pithadia