This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS92515-Q1: Unable to open simulation of TPS92515-Q1

Part Number: TPS92515-Q1


Tool/software: WEBENCH® Design Tools

Hi,

I'm having issues with opening a simulation or design of the TPS92515-Q1. I have tried clicking the WEBENCH links on the TPS92515-Q1 and also creating a new design in WEBENCH. I've tried different input voltages, different LEDs, and still can't get it to launch. WEBENCH seems to open fine. Does the model actually exist in the software?

For reference, here's what I'm trying to simulate:

Vin (min) = 22.4V

Vin (max) = 33.6V

LED Vf = 11.2V

LED If = 1A

LED Rd = 0.58 Ohms

Thanks for your help.