This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642: Confuse about mmWave Sensing Estimator

Part Number: IWR1642


When I use mmWave Sensing Estimator to estimate the maximum detecte range on IWR1642, I confuse about mmWave Sensing Estimator

Keep all other settings, change number of RX Antennas.

1 Rx antennas & 1 Tx, maximum range is 75.41m

2 Rx antennas & 1 TX,maximum range is 84.66m

3 Rx antennas & 1TX, maximum range is 99.25m

4 Rx antennas & 1TX, maximum range is 95.05m

It confused me that 3 Rx antennas can get the maximum range