This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01495: TIDA-01495

Part Number: TIDA-01495


We are planning to modify this design to work with output 28 V and Current 24A..

Please suggest suitable changes to incorporate with the above required output level

  • Hi Ramakrishna,

    This will change the magnetic components and power components. Even the PFC section will get changed, as the power has increased. Please go through the design guide and use the design procedure given in it to modify the components according to your specifications.

    Regards,

    Salil