Hi. Working on a common pinout RS232 / RS422 / RS485 design where the respective transceivers will be disabled as required. Came across TIDA-00540 and concerned if this will function as noted due to the internal 5k pull-down resistors that are present on each of the RS232 inputs. Or do these internal 5k pull-down resistors also get disabled when the RS232 transceiver is disabled / powered down?
On this same note, do all TI RS232 transceivers disable this 5k internal pull-down during power down / disabled mode?
Concern is that the 5k pull-down resistors present inside the RS232 transceiver will affect the signal integrity / biasing of the shared RS422/RS485 transceivers.
Please advise.
Thanks and happy holidays!!