Part Number: PMP10116
Other Parts Discussed in Thread: LM2596,
Hi,
I have following doubts with respect to this design.
1. Value of DNP: What should be values of DNP resistors and capacitors? Or else to be shorted or to be kept open?
2. 5V Auxiliary input: Suggest me the circuit to get 5V supply from this design. I think 15V Aux supply is available. Shall I use LM2596 for getting 5V output? Or do you suggest any other circuit?
3. What changes I should do in this design to get output of 150W and 180W?
4. Can I use PWM for dimming instead of 0 to 10V dimming? If yes, What should be Maximum voltage of PWM signal?
5. Is it 'dim to Off' kind of dimming? I mean, In 0 to 10V dimming, at 0V will driver turn off the output supply?
Thanks,
Regards,
Amit