This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01212: TIDA-01212: problem of sce of tida 1212

Part Number: TIDA-01212


HI Sir,

i am working on the bidirectional IR projects

IN the scp project the defaul io pin is 28,29

however, in training

in 7:35, it mentions that we need to use IO 5,6,7 as the IR tx for high driving strength, how do i need to adjust the io pin in the scp ?

thanks

Jeff

  • Jeff, hello. Your question has been forwarded to the owner of this design, however, he is still out of the office on holiday. He will return to the office on Monday, January 7th and you should hear from him shortly thereafter.

    Best Regards,
    J. Fullilove
    Texas Instruments
  • Jeff,

    please open the File "HCACapTouch_IRLED_7bits.scp" from TIDA-01212 under Sensor Control Studio and then click on I/O Mapping (in the left pane, under the separate project tasks).
    Now you can see all used I/O functions and the DIOs used; here you can change their Pin assignment as you need them.

    Regards,
    Milen