This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP5123: PMP5123

Part Number: PMP5123

Hello,

Does PMP5123 cater to an input of 8 V dc to 36 V dc for an output of 12V/8A.

Because I need 8 amps as output.

Regards,