This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDA-00951
Having looked through the schematic, I have several other queries:-
Hi Francis,
Please find my reply below.
1. The heatsink were custom parts, so do not have a ordarable part for them. Larger heatsinks are only for thermal reason at full load and minimum battery voltage condition. However you can reduce the size depending on your fan speed.
2. For U11, please use TPS62163 instead of TPS62160.
3. For the high voltage side our test did not indicate need for snubbers. In your simulation did you look at the charging or backup mode?
Best Regards,
Ram