Tool/software: TINA-TI or Spice Models
Hi,
In "AC transfer characteristic" we normally use a generator which produces a constant amplitude for all frequencies.
Is it possible instead to import some file, or manually enter frequency and amplitude for sweep sine?
Maybe is it even possible to make some "block" or macro model which converts input sine into a sine with different magnitude and frequency based on such a table?
We have a system in which, when we drive actuator with sine wave, sensor produces a signal with different amplitude and phase (the "plant Transfer Function"), and we can easily obtain this transfer function in a table form:
| freq | Mag, dB | phase |
| 1000 | -19.39 | -81.45 |
| 950 | -18.56 | -73.03 |
| 900 | -17.49 | -63.59 |
| 850 | -16.6 | -56.63 |
| 800 | -15.54 | -47.25 |
| 750 | -14.61 | -37.31 |
| 700 | -13.59 | -27.96 |
| 650 | -12.59 | -17.88 |
| 600 | -11.47 | -6.99 |
| 550 | -10.38 | 3.86 |
| 500 | -9.21 | 15.75 |
Some transfer functions are simple and COULD be created using R-C-L filters in TINA (like red plot below), but some are difficult to create using filtering (blue):
The goal is to create analog compensator using OPAMs and R-C-L filters to have good gain, broad bandwidth feedback based on plant transfer function,
which of cause is easier and quicker in TINA than on breadboard with real components
Thanks!
Igor