Part Number: TPS7A49
Other Parts Discussed in Thread: TPS7A4001
Tool/software: WEBENCH® Design Tools
Hello
i have some problem with TPS7A49 ic simulation
i tried some different values of Vout and always i get big error voltage
for example, with Vin = 30, Vout = 15 and Iout = 0.05 i get 14.4V instead of 15V (stady state)
it's gets worse when i asking for higher Vout...
by the way, i see the same problem on my PCB board
my Vin = 30 and Vout = 28. i get correct Vout only when there is no any current consumption
with 3mA load, the output voltage is dropped to 26.5V
I'd be happy to get help with this...
thnks
david