Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
Hello,
When I try to run a PSpice simulation under temperatures like -40, 0, 50 and 80degC, using the TPS92638-Q1 PSpice Transient Model (Rev. A), I'm receiving an overflow message.
"Overflow in device X_U1.D_UCR3_D11"
I included T_ABS=27 in the D_D diode inside the PSpice model and the device changed.
"Overflow in device X_U1.X_UDgSC3_U48.d_d10"
I know that "apart from Thermal Shutdown and Thermal foldback, other temperature effects are not modeled", but the behavior of the LEDs and the rest of the circuit is important for me.
Do you have any tip on how can I fix it?
I connected a power supply in the TJN pin, with the recommended values, and already tried a lot of different simulation settings options.
Thank you in advance,
Julio Costa